Part Number: TPS25820 Tool/software: Hi,
I am developing a smart cable and found that TPS25820 is a good choice. However, from the datasheet I couldn't find detailed design guide lines for using the VCONN feature. Of course it is all according to the…
Other Parts Discussed in Thread: TPS25820 Hello,
Using TPS25820 & Type C to Type C connection, I want to understand the current limit after attach as per USB PD3.2. In USB2.0, it is 100mA before enumeration. Does same apply here ?
Part Number: TPS25820 hi Teams:
Please help review the schematic diagram below. Thank you.
1. The input is USB-A and the output is USB-C. Now, it is required that the output USB-C has no power when not connected to Device, and only when connected to…
Part Number: TPS25820 Other Parts Discussed in Thread: TUSB1210 , TPS25750 Hello,
I plan to design a type c interface with TPS25820 and TUSB1210. The requirement is
1. support up to 3.0 version.
2. support host and devcie mode as well as USB 2.0 OTG devices…
Part Number: TPS25820 Other Parts Discussed in Thread: TPS65988 , TPS65987 , TPS25750 Hi PD-team,
My customer would like to confirm TPS25820/1 support dead battery test.
Regarding to the datasheet, It seems they doesn't support it comparing TPS65988…
Part Number: TPS25820 I have created a design using a TPS25820 with a USB-C connection. As I was reading through the data sheet I noticed on page 19 of the data sheet the following:
" However with DCP implementation the port will not support any data…
Part Number: TPS25820 Is it possible to obtain and share with me a copy of the TPS25820 certification body report for IEC60950-1?
Thank you.
Best Regards,
Emma,
To get charging to work, I had to use a cable with one CC line connected through (as in the drawing you provided). If the cable has both CC lines connected, the TPS25820 never sources power.
My application requires the phone be a data host, not…
Part Number: TPS25820 Hi,
the TPS25820 mentions a discharge resistance in the table under OUT-DISCHARGE, is this something that is internal to the part?
If I understand this feature is to allow the discharge of the output rail when a sink device is not…
Part Number: TPS25820 Other Parts Discussed in Thread: TPD6S300A Hi team,
Do you have replacement for ONSEMI FUSB251? We want to use the function of Moisture Detection on CC and SBU Pins.
TPS25820 seem not like it. Do you have any replacement part number…