Thanks Arnold!!!
Thanks for your notice:)
The Name of function we called is bit confusing for you...its seems like it is used for BQ7961X AFE. Actually This function Name i was used in BQ7961X AFE earlier Project.
But now i am working on BQ79718…
Part Number: LM3410-Q1 Other Parts Discussed in Thread: LM3410 Tool/software: Hello,
My customer is looking for an automotive LED driver IC that supports the following conditions.
- AEC-Q100 LED driver
- VIN : 3V, VOUT : 18~24V (LED 9EA)
- Iq…
Hi Takuma,
Takuma Fujiwara said: The numbers that we have are what was posted in April 17 on this thread.
4
READ
1024000
1514445
12.11556
5
READ
1024001
1504268
12.03414
The max throughput in the table is 12Gbps…
Part Number: TPS1HTC100-Q1 Tool/software: In the datasheet for TPS1HTC100-Q1, page 17 and 18 the diode clamping is mentioned on drain to source(Vds,clamp), but in the diagram it is given between drain and gate. Could you please confirm about that.
Additionally…
Part Number: LM25037-Q1 Other Parts Discussed in Thread: UCC28700 , LM25037 Tool/software: Hi Team,
Need support to design DC to DC isolated -20KV @4W output. Input 8 to 18 V DC.
Part Number: CDCE6214-Q1 Other Parts Discussed in Thread: ADC3683 , Tool/software: Hello,
We plan to use CDCE6214-Q1 with ADC3683.
We use TICSs Pro to configure the register of CDCE6214-Q1 as following :
1. Ref freq diff of 60MHz / PFD freq = 60MHz…
Hi Kyle,
Kyle Kim said: 1. How much current will flow in sleep mode if I use extra LDO? (The datasheet states less than 20uA, is that right?)
Datasheet says 18 uA max and 7 uA typical. I have not heard anyone report that this is not correct.
Kyle…
Hi Fabian,
1. I don't think the CMC and inductors need to achieve a certain ESD rating.
2.The setup should be a specialized equipment. You can also check section 4.2 in the 713 reference design as a reference.
3. The TPD3S713x-Q1 device can withstand…
Hi Frank,
Thank you for your question.
1. It comes from internal circuit- confidential. As FAQ, it is ~5.3V
(+) [FAQ] DRV8714-Q1: [FAQ] DRV8705/6-Q1, DRV8714/18-Q1 Offline diagonastic - Motor drivers forum - Motor drivers - TI E2E support forums…
Part Number: UCC14141-Q1 Other Parts Discussed in Thread: UCC14141EVM-068 Tool/software: Hello,
Are the analog grounds (pins 1,2 and 5) and power grounds (pins 8 through 18) on the primary side connected together internally? Likewise, is the VEEA analog…