Part Number: TUSB1044RNQEVM Tool/software: Hi
TUSB1044RNQEVMW uses a 5V power supply. If power is taken from the Type C plug and 100W is provided to the device connected to the Type C socket, does it require the addition of a PD controller with DRP function…
Part Number: TUSB1044RNQEVM Tool/software: Hi, we are using TUSB 1044 for USB 3.2 gen 2 to DP (10gbps using all 4 lanes). Going through the specifications sheet, dont see any mention on its compatibility of P/N swap within a pair.
Can you please confirm…
Hi Yingjiao,
I will mark this thread as resolved and work towards updating the EVM user's guide on TI.com. If you have any questions, feel free to respond here and it will re-open the thread.
Best,
Shane
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB1104 I tested TUSB1044RNQEVM because I want to design the USB redriver.
But I found the problem.
I don't want to use the USB 1:2MUX, then I want to set the USB 4 lane setting(RX1/TX1,RX2…
Part Number: TUSB1044RNQEVM I got a TUSB1044RNQEVM from TI distributor. The board version is HSDC008B. How could I get the schematic file (.pdf is OK) for this version of EVM?
The schematic file available in the TI website is only for version HSDC008A .…
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB216I Hi Sir,
My customer want to design a 10m active cable for type-c signal.
1. Is it ok to use TUSB1044EVM's circuit to meet customer's requirement? Where do we have to put the redriver…
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB1044 , TPD6S300 , TPD1E0B04 Hello TI experts,
my customer considers TUSB1044 for their new product, and I have one question.
in TUSB1044 EVM schematic, there is one TPD6S300 for ESD protection…
Part Number: TUSB1044RNQEVM Other Parts Discussed in Thread: TUSB1044 Hello TI experts,
My customer considers TUSB1044 for their new product, and they want to get artwork file of EVM.
they use Allegro, so it would be good if you have a file which extension…
Part Number: TUSB1044RNQEVM Hello,
The EVM user guide includes this note: "If testing DisplayPort only, or if bypassing VBUS power, the EVM must be powered via J4 (5 V, 1-A input)."
I'm not sure I see how VBUS can be bypassed, is there a resistor…