Part Number: TUSB2036 Hi,
Our customer has requested a schematic review. Could you please review if there are any defects in the schematic? We are sorry to trouble you, but we would appreciate your cooperation.
Also, is my understanding correct that the…
Part Number: TUSB2036 Other Parts Discussed in Thread: TPS2044 , Hi,
When the connected device latches up, Other than TPS2044 overcurrent detection(Datasheet Figure 9), is there any way to turn PWRON# high? Also anything other than how to make the Reset pin…
Part Number: TUSB2036 Hi,
There is a description of the Reset sequence for Power on, but I couldn't find the description for Power down. Are there any precautions for power down?
Best Regards,
Nishie
Part Number: TUSB2036 Hi,
I used the TUSB2036 to connect two downstream port to the CPU. In the last version, I forgot the 15K pull down resistors. With manual assembly of these resistors, the problem resolved. I made a new version of PCB, but now the…
Part Number: TUSB2036 We are using a TUSB2036 as a hub and it is being mis-identified as a HID, this appears to be an intermittent fault and will sometime innumerate correctly, has anyone else had this issue
Part Number: TUSB2036 Hi,
1. Are DP0 and DM0 pins dedicated to the host device? 2. If the host device is a tablet, can the device connected to the Downstream port be checked from the tablet by the device manager? 3. Is there a notification (signal) from…
Part Number: TUSB2036 Dear Team,
We have used TUSB2036VFRG4 IC in one of our current design. We are facing an issue on the speed of the USB which is configured.
Our device is working at USB 2.0 (480Mbps - High Speed). But TUSB2036VFRG4 downstream ports…
Part Number: TUSB2036 Attached is the schematic I put together on the new design.
R49 is DNP
After I connected USB cable to J4 I am not able to read anything on the USB port.
Mostly I don't see any device plugged into the computer.
After checking U9…