Part Number: TUSB8041 Tool/software: Hi Team,
We are planning to use TUSB8041IRGCT usb3.0 hub in our design. can we use the output channel as usb2.0 only as well as usb3.0? in our soc side, there is only one usb port (3.0) and we have to use this usb…
Part Number: TUSB8041 Hello.
I checked the operation by configuring downstream 3.x A type circuit using the TUSB8041.
We connected a sensor with a C type interface to this board using an A-to-C cable.
After that, I added the cable circuit to the TUSB8041…
Part Number: TUSB8041 Other Parts Discussed in Thread: TPS2069E , TPS2001C Tool/software: Hi all,
Just need a sanity check I think.
I've had a lurk about but can't find whether or not I can bus-power a TUSB8041 within specification or not.
As…
GARETH OU said: Adjust the value of USB_R1, adjust it downward to 9K, right
correct.
GARETH OU said: customers have tried to adjust it from the SoC side (through BIOS),
what did customer try to do though BIOS? improve USB2 eye?
to improve USB2 eye, you…
Hi Santhosh:
For USBET20 tool, please take waveform with CSV format, then load *CSV file to USBET20 tool.
USB_R1 will affect the drive current on DP/DM which affect the driver strength at USB2.0 speeds.
Regards
brian
Part Number: TUSB8041 Other Parts Discussed in Thread: TIDA-00288 Tool/software: Hi Brian.
The customer wants to make a design: the upstream interface is type C, and then connected to TUSB8041. But the customer doesn't know what the specific wiring should…
Part Number: TUSB8041 Hi,
I'm a student and i'm trying to create an HUB using TUSB8041 as the main IC. For that, it would be very helpful if i could get the gerber file of the TUSB8041 EVM evaluation board. Thank so much for your attention.