Part Number: TUSB8044A Other Parts Discussed in Thread: TUSB8042 , Hi
Please help support and suggest specs and designs.
Could you recommend a hub with 2 ports?
You can see our original plan as below figure.
Thanks
Part Number: TUSB8042 Other Parts Discussed in Thread: TUSB8043 , TUSB8044 , TUSB8040 , TUSB8041 , Because of assurance of supply (AOS) issues I am looking at loading a TUSB8044[A] or TUSB8043 in place of a TUSB8042RGCT part currently on my board.
It looks…
Part Number: TUSB8044A Other Parts Discussed in Thread: TUSB8044 Hi Team
We are using TUSB8044, just want to have one clarification why 1M ohm resistance is required bet two XI and XO pin
Kindly refer to above wave shape at XI and XO pin and let me…
Part Number: TUSB1064 Other Parts Discussed in Thread: TUSB8044 , TDP0604 , , TUSB8044A , SN65DP159 Hello,
I am working on the HUB design with 2x USB 3.X and 1x HDMI outputs.
I selected the TUSB8044 for HUB (even there are 4x USB3x).
Also, I need to find…
Part Number: TUSB1064 Other Parts Discussed in Thread: TUSB8044 Hi David Liu,
Thank you for the answer!
Unfortunately, the MCDP2900 is obsolete device, so I can not use it for a new design.
It is really unbelievable there are no such devices on the us…
Part Number: TUSB8044 Hi Sir,
About the SMbus mode, is it only support 100KHz data rate? how about 400KHz?
My customer is asking if they can use both 100KHz & 400KHz to control hub or only 100KHz is workable?
Please help to advice.
Thanks
Part Number: TUSB8044 Other Parts Discussed in Thread: TUSB8042A Hi
I am planning to use TUSB8044 for our USB hub product.
Please help to check schmetic if ok or not.
TUSB8044 USB2.0 hub.pdf
Thanks,
Edgar
Part Number: TUSB8044 Hi Team,
Could you update the difference between non-A version and A version?
I saw in another E2E post that "We will have a document releasing soon on how to transition from TUSB8044 to TUSB8044A. This will highlight the differences…
Part Number: TUSB8044AEVM Other Parts Discussed in Thread: TUSB8044 Hello,
Actually I'm designing a hub based on TUSB8044. I need the schematic and PCB files of evaluation board to verify my design. I'd like to ask you for these files. It will help…