Part Number: TVS2701 Tool/software: Dear Support,
Can you tell how to properly Fuse the TVS2701 TVS diode ?
Vin normal operation 24V 1.25A -> 30W , max current 2.25A -> 54W
Can you tell how to size the fuse, so that the fuse blows before the…
Part Number: TVS2701 Other Parts Discussed in Thread: TVS2201 , STRIKE Hi Team,
we are currently using the following scheme for reverse polarity where TVS is after RPP.
The input is 24VDC from standard industrial supply.
But now we want to ESD protect…
Part Number: TVS2701 Other Parts Discussed in Thread: TVS3301 Hello,
I would like to simulate TVS2701 and TVS3301 on LTSpice, and thus need the SPICE model.
The one available to download from the TI website is encrypted, can I get a model that is not…
Part Number: TVS2701
Dear Technical Support Team,
I got TVS2701DRBR and this marking is "PPTP".
Is this correct marking? Is this fake chip?
According to the datasheet, the marking of T VS2701DRBR i s "1PTP".
Best Regards,
ttd
Part Number: TVS2701 I want to recommend TVS2701 to customer and replace 3.0SMCJ26CA-AU_R1_00001,SMC ! Please help to confirm if there is an error ,THX
Part Number: TVS3300 Other Parts Discussed in Thread: TVS2700 , TVS2701 Tool/software: Input Voltage is of 28V and current is 2A. Power Module Voltage Range: -1V to 6V
Which is the best method to be followed:
Reverse.tif
Kindly suggest TVS diode and SCHOTTKY…
Part Number: TVS2701 Hi team,
One of my customer considers to use TVS2701 and provided a question.
The datasheet’s layout example shows that input trace width seems to be same as input lands.
Is there concern that trace width which is wider than…
Part Number: TVS2701 Hi,
I am developing a device which need protection according to MIL-STD-1275E: everyspec.com/.../download.php
The device need to withstand a 100V surge and a ±250V spike. I have found a solution to withstand the 100V surge test, but…
Part Number: TPS2640 Other Parts Discussed in Thread: TVS2701 Hi team,
1)
can you tell what is the purpose and how to select schottky diode on output, page 38 figure 11-1 in Datasheet?
2) In what scenario can we use bidirectional TVS2701 instead of SMC…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation and Temperature
Top…