Bala,
Clemens is correct that if you want to do this with one device then the TXS0102-Q1 is the best option, but will have limited speed.
UART can range in speed but typically is lower speed and the TXS0102-Q1 device should be able to support your…
Hi Pavel,
Thanks for your reply,
I have checked the threads referenced by you above,
In our design we are not using any such HDMI protection chip. For the differential line of HDMi we are using Common mode choke with ESD protection , TXS0102…
Hi Kato-san,
You should use a dual-supply voltage translator like TXS0102, which has V CC isolation feature – if either V CC input is at GND, both ports are in the High-Impedance state.
Hi Nirav-san,
Our customer will try to use TXS0104E with I2C or SPI interface.
By the way, according to the data sheet of TXS0101 and TXS0102 these parts support the partial power-down mode. In addition, it seems that TXS0104E supports it in the following…
Sonu Verma said: I have to interface MSP430F5325 with two I2C salves whose offset voltages are 3.3v and 5.5v
For interfacing a 3.3V I2C device to a 5.5V I2C device I suggest using an 2-bit (SDA and SCL) open-drain voltage level translator like the TXS0102…
Hi Brian,
Thank you for your fast reply.
I'm sorry, but the TCA9517 doesn't operate 1.8V, especially B port.
How about the TXS0102?
Regards,
Naoki Aoyama
Hi Hariram,
Your issue is likely hardware related and due to the direct logic level incompatibility between the LaunchPads and PGA450-Q1. The PGA450-Q1 UART channel requires 5.0V logic level, but the LaunchPads can only operate at 3.3V logic level. You…
Section 6.3 says that the I/O port voltage must not exceed Vcc.
A two-channel digital switch with Ioff support would be the TXS0102, or TXB0102/TXB0302.