Part Number: DRA72XEVM Hi,
I need to start cross compilation of Android for TDA2ex. Before that I would like to check with TI team if this is possible...?? (Android latest or previous versions)
I would like to know if there is any limitation. Once successful…
Part Number: DRA72XEVM We are running an Linux application which has an POSIX pthread running every 50 ms. This is executed on the A15 core of TDA2SX. This thread gets scheduled every 50ms initially for an hour. After an hout the thread scheduling gets…
Part Number: DRA72XEVM Hi TI,
Based on the requirement of H.265 encoding and H.265 decoding and as we are using Vision SDK could you please advice if the latest version of Vision SDK supports H.265 video encoding and decoding
Regards,
Raghav
Part Number: DRA72XEVM
Dear TI experts,
I was trying to do TIDL inference using app_tidl code with some modifications to handle the N channels inputs to do inference.
I observed when I gave the input tensor of size [1, 400 ,248,296], the inference results…
Part Number: DRA72XEVM Hello,
We are running the application on the custom board having TDA2xx SoC and Vision SDK 3.0.7
The usecase is as below:
Capture -> VPE -> Display_Video
For few minutes initially the display is coming properly. However…
Part Number: DRA72XEVM Hi TI Forum,
We are using custom board having TDA2xx SoC. We are using Vision SDK 3.0.7
We have a requirement wherein we would need to switch between splash screen and Reverse camera display during boot till completion of Linux kernel…
Part Number: DRA72XEVM Hello,
I'm implementing memory protection on the C66x DSP side.
I'm trying to read the parameters of access done to the memory protected by the XMC but it returns zeroes.
I'm protecting a memory by setting XMPAXH and XMPAXL…
Part Number: DRA72XEVM
Hello,
I would like to connect to the C66 DSP on the DRA72xEVM board via the DSS scripting. My ccxml file looks as follows:
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0…
Part Number: DRA72XEVM Hi TI Forum,
We are using custom board having TDA2xx SoC. We are using Vision SDK 3.0.7
We have a requirement wherein we would need to switch between splash screen and Reverse camera display during boot till completion of Linux kernel…
Part Number: DRA72XEVM Hello,
I'm implementing the memory protection on the C66x DSP side. The memory protection works but in order to have it working I had to copy functionality from the dsp_xmc.h file. That's because the libraries in the pdk_dra7xx_1_0_10…