Hello!!
I have a OMAP3730-module and need to install a real-time patch. Originally, a kernel based on the vanilla kernel 2.6.32 (with special VAR-SOM patch PSP 03.00.01.06) was installed, so we decided to use a omap-patch (03.00.00.02) and the 2.6…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: GPCCHEM , BQ40Z50 , BQSTUDIO , BQ78PL116 Hi,
We are using the BQ40Z50-R2.... The Full charge capacity of the production packs seen jumping to zero AH, the primary suspect we are having is the…
Arvind,
If you want to modify the circuit for a different transfer function, you can use excel calculator tool below
/cfs-file/__key/communityserver-discussions-components-files/14/2112.Voltage-Scaler-Calculator_2800_1.02_2900_.xlsx
Use Non-inverting…
Other Parts Discussed in Thread: OMAP3530
A TI Customer is using the OMAP3530 with the TWL4030 companion chip. Has been trying to adjust the USB drive strength using the VBUS_EN_TEST and ID_EN_TEST registers. However they seem to be unable to unlock…
Other Parts Discussed in Thread: LM3S5632 Dear sir,
I have one doubt till today i did not get satisfied answer any of them please any one solve my doubt.
In some micro controller has multiple crystal oscillator connection let say
1) primary oscillator…
Hi Badri,
Thanks for your reply.
Here is my Use case...
/* Capture (YUV422I) 16CH D1 60fps | | NSF (YUV420SP) | +------------+ | | DEIH DEI | | | +----------+ | | MERGE | ENC (H264) | | TS STREAM (UDP) */
Here are the detailed statistics...…
Other Parts Discussed in Thread: OMAP-L138 Hi,
Would like to report some problems that appears to be the limitation of LCDC DMA capability.
First is regarding a bit “LCDEN” for enabling DMA transfers, documented in L138 TRM SPRUH77 page 1000, 1001…
Hello Susa,
The Wiki is being discontinued. You can try to download with Device Monitor instead.
/cfs-file/__key/communityserver-discussions-components-files/538/CC2650RC-Getting-Started-with-Development-_2D00_-Texas-Instruments-Wiki.pdf
/cfs-file…
Other Parts Discussed in Thread: BQ27510-G3 , BQSTUDIO Hi all,
In one of our designs, we are using the fuel gauge BQ27510-G3.
We have successfully completed the optimization cycle of this fuel gauge using BqStudio software and generated the golden…
Part Number: AM3351
hi,
i am using DDR3 of MT41K512M16HA-125ATR for my custom board .
i am attaching Datasheet of DDR3 MT41K512M16HA-125ATR:
MT41K512M16.pdf
According to EMIF tool it is generated Below timings and i modified board.c file according…