Recently purchased an MSP-FET430U14 programmer and the CD will not run on my computer. I've downloaded and setup IAR workbench but have not been able to find any drivers for the programmer. Can someone please point me in a direction?
Thanks.
Hello,
I have a brand new MSP-FET430U14 which is no longer functional after updating the firmware.
I first loaded the IAR Embedded Workbench 5.4 Kickstart on a Windows XP SP3 machine, and then connected the USB Debug Interface which was recognized successfully…
Thanks Katie. I will do what you suggest to remedy the compile issue.
However, my larger issue is that I can't program the Launchpad from the PC. I've tried to burn the binaries that are provided in the examples directory but when the MSP430Flasher…
Howard Tang said:
I need to buy a MSP430 and it will be mounted on PCB with my power management unit, which type of packaging should I buy?
You will need to select the ideal MSP430 for your application based on your requirements. You will know these…
Hi,
Thanks for the reply. I was downlaoded this IAR Embedded Workbench Kickstart software from the website which prompted from installed CD. The software descrption as stated below where the GUI without MSP430F4152 device. Any idea for me to download the…
Here are some recommendations:
1. Try running th code example "msp430x20x3_sd16A_01.c" from the following zip file "as-is": http://www.ti.com/lit/zip/slac080
To test the above code example, tie the A1+ input on your board to Vcc and…