Part Number: PROCESSOR-SDK-AM335X Tool/software: I have found processor-sdk-kirkstone-09.02.01.09-config.txt and some other xxx-config.txt,which version is newer than processor-sdk-09.01.00-legancy-config.txt. But in the release note not clearly indicated…
Part Number: PROCESSOR-SDK-AM335X Tool/software: Hi,
I want to connect a TFT that works with SPI 3-wire. When in device tree add spi-3wire., I have this error in dmesg.
spi spi0.0: setup: unsupported mode bits 10
Does the AM335x processor support 3-wire…
Part Number: PROCESSOR-SDK-AM335X
Tool/software: ti-processor-sdk-rt-am335x-evm-09.01.00.001
I'm trying to edit the kernel config of the yocto build for the Processor-SDK-Linux-RT v09.01. I've setup the yocto environment with the processor-sdk…
Part Number: PROCESSOR-SDK-AM335X Tool/software: If there is the plan to support TI SDK 10.0 for am335x, when will this version be released?
Thanks
Xulin
Part Number: PROCESSOR-SDK-AM335X Tool/software: Hi,
I used the am335x-evm.dts to make the changes. I deleted all configuration about LCD and added SPI display and added a driver to Kernel. In dmesg I showed the message about the display starting but…
Part Number: PROCESSOR-SDK-AM335X Tool/software: This is related as it deals with the same SDK and Processor. At some point as I was trying out this updated SDK the bitbake **devshell** stopped functioning correctly.
A command like `bitbake -c devshell…
Hello Daisuke-san,
Daisuke Maeda said: Does TI support the PDK packages on the git repository? Could you answer the PDK questions on E2E?
Not for the devices listed in the announcement you referred.
Regards,
Jianzhong
Part Number: PROCESSOR-SDK-AM335X Tool/software: I also posted this question worded differently in an am335x SDK thread as this one did not show up in the search, (but I did get here from an external Google search).
I am not able to complete the make…
Part Number: PROCESSOR-SDK-AM335X Tool/software: Hi all:
I copied 6114.lcd.zip to my u-boot/driver and make u-boot.
I download u-boot to my sdcard.(I used sdcard to bootup)
Each time I enable lcd function, console will show "Trying to boot from MMC1…
Part Number: PROCESSOR-SDK-AM335X Tool/software: getting this error while compiling the mind connect base code on tisdk9.1 -
Log data follows:
| DEBUG: Executing shell function do_compile | -- The C compiler identification is unknown | CMake Error at CMakeLists…