Part Number: ADC12D1620QML-SP Tool/software: Hello, About pin descriptions, there are differences between ADC12D1620QML-SP datasheet and the SMD document as follows. Which is true? 12205.pdf adc12d1620qml-sp.pdf Best regards, K.Hirano
u-boot-files.tgz.base64.txt
Prashan,
I cant upload file in binary format, so I convert in base64.
Use the following commande to get the archive:
base64 -d u-boot-files.tgz.base64.txt > archive.tgz.
So I include the tisdk u-boot base files, the…
Hi Margaritha,
What could be the reason that mdiscalar and hdiscalar elements behaving differently?
One thing I observed that while using mdiscalar element 2 out of 3 frames capturd are full of grains as shown in the snapshot below
yuv file :…
Part Number: TDA4VM
Tool/software:
Hello,
We are trying to run out model on EdgeAI 9.20.07 . https://github.com/TexasInstruments/edgeai-tidl-tools/tree/09_02_07_00?tab=readme-ov-file .
We have observed issue with Matmul layer on target when…
Hi,
It may not need to run in FDU mode. You can add MSPM0_BSL_GUI.exe in SDK installation folder\tools\bsl\BSL_GUI_EXE. Modify the attach file name from .txt to .exe
MSPM0_BSL_GUI.txt
Then run the .exe file. In MoreOption->Update XDS110 firmware…
Hi Stefan,
I've attached the zImage and the modules for the corresponding image. Please try this out and let us know if it works. Copy the zImage to the boot folder in the rootfs partition and the modules to the lib/modules folder in the rootfs partition…
Hi,
I mean I can play it in VLC, but it play not smoothly. when I use the Elecard StreamEye Tools to play it , it is smoothly, i
I have uploaded the video . Because i want to upload the video ,so i have to change the file`s expanded-name to txt, it…
Hi Patrick,
nothing is wrong, we found out an unexpected bug in the software. The correct version will be updated by today on the website. In the mean time I can share with you this version in advance. Could you please try it out and check if you face…