Part Number: TMDXIDK5728 Tool/software: Linux I want to use Big Data IPC to process an image on DSP. The image will be captured by ARM Linux and then the shared memory will be filled by the image pixels. Can I use C++ on DSP side?
Working with images…
Part Number: TMDXIDK5728 Tool/software: Linux Hi,
I was able to complete the IPC example via Linux SD card method. If I want a better understanding of what's happening in the code, how do I debug it or step through it, similar to how I would in CCS? How…
Part Number: TMDXIDK5728 Tool/software: Code Composer Studio Hi Support,
We will use a Redis server for our application. This application comes with the Linux SDK kernel. I am using Linux SDK 5.2.0.10. I am using Ubuntu 18.04 LTS.
I am able to run a Redis…
Part Number: TMDXIDK5728 Tool/software: Linux I am attempting to run the pre-built example applications from inside the Linux-RT filesystem. All of the example files are ELF 32-bit LSB executables, which cannot be run on a 64-bit Linux OS. What am I missing…
Part Number: AM5728 Other Parts Discussed in Thread: TPS659037
Team,
Regarding the OSC16MCAP Alert:
-Could you please provide a picture to show the best positioning of the 2.2uF 6.3V that need to be added at the OSC16MCAP pin?
[EDITED] After double checking…
Part Number: TMDXIDK5728 Tool/software: Linux Hello,
I am running the newest Linux SDK on a SD card and I am root debugging through my JTAG to USB XDS100v2. I have a PCAN Connector attached to my J38 CAN header pins. I am able to send CAN frames FROM…
Part Number: TMDXIDK5728 Tool/software: Linux Support,
I am working with the AM5728 IDK; I am running Linux directly on the board with the SD Card u-boot. I am using the SDK release from mid-December, v5.2.00.10.
I am trying to use "make menuconfig" and…
Part Number: TMDXIDK5728 Tool/software: Linux Hello Linux Support,
I am able to run the makefile MessageQ example. ( e2e.ti.com/.../2839504 ) I want to build a custom application using the MessageQ, with IPC between the Linux ARM core and the RTOS DSP core…
Part Number: TMDXIDK5728 Hi,
We have an IDK board that just stopped booting SD Cards. It previously booted SD cards correctly. We have a few IDK boards and we verified another IDK board can boot the SD card fine.
We can tell the IDK board is booting from…
Part Number: TMDXIDK5728 Tool/software: Code Composer Studio Hi
I want to offload a section of my code on DSP for the sake of acceleration. Is it possible to define the CCS project on ARM and then do a specific part (or function) of the code on DSP?
…