Part Number: OPA455
Other Parts Discussed in Thread: OPA551, OPA462, INA228, OPA2192, TINA-TI, OPA454, OPA1622
Hello TI expert
1.There is a piezo driver project need to design, below is the piezo actuator information
the capacitors min is 0.15uF and max is 15uF, the resonant frequency is between 40Khz to 135Khz,
maximum power consumption is between 0.8W to 34W, maximum travel range: At 0 to 120 V, The decice
current is calculate Imax =Pi *f* C*Uvpp.
2.A ccording above, If choose the OPA455 driver a device capacitors is 3.1uF, voltage is 100V the maximum frequency is 46Hz.
If increase the frequency the OPA455 cannot achieve, it may be need extend the current to achieve.
3.My question is how to use OPA455 extend the current or other solutions? Can you suggest some typical circuit ? If the
circuit can select output sine wave, square wave or triangular wave is the best.