Part Number: OPA454
Other Parts Discussed in Thread: TINA-TI
Hello TI support team,
My application is to produce a square wave to charge a capacitor (around 0.4uf), and here is the circuit I plan to use:
The input DAC_P01 is connected to output of a DAC and the voltage ranges from -5V to 5V. The output P01‘ voltage is required from -45V~0V~+45V (60hz) according to DAC_P01.
Maximum current is around 800mA. Adjustable resistance VR1 can be set from 0Ω to 100KΩ.
Now the questions:
1) Is the circuit above capable enough to charge the capacitor?
2) When EN is 3.3V the circuit works normally, and when EN is GND level the circuit shutdown?
3) How to choose transistor Q1&Q2 and resistor R3&R6&R8? what's the key parameter need to be calculated first?Any mos to recommend to replace transistor?
Thanks in advance for your answers
Lahm