This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer uses LM393B as voltage detection.
when there is input power and ambient temperature is at >0C, it works normally as below.
CH1: Vo
CH2: IN+
CH3: IN-
ch4: Vcc(VBUS)
when there is input power and ambient temperature is at 0 - -30C, LM393B works strangely as below.
Vo has strange pulse but IN+ is lower than IN-.
the schematic is as below.
from Datasheet, LM393B should work at >2V and -25C.
Can you help check what happen?
BR,
frank
This circuit uses invalid input voltages; see the VIVR specification in the recommended operating conditions.
This is explained in more detail in the Application Design Guidelines for LM339, LM393, TL331 Family Comparators:
The specified LM339 Family input voltage range (VICR) is 0 V (relative to the negative supply pin) to VCC – 1.5 V at room temperature. However, the actual upper input voltage range reduces by -4 mV/°C at cold temperatures. Therefore the specified LM339 Family full temperature range common mode range is 0 V to VCC – 2 V to account for this reduction. The VCC – 2 V range is strongly recommended for use in all designs.
Also, the second comparator's inputs must not be left floating.
To avoid that pulse, you must use a comparator with rail-to-rail inputs. If you do not want to change the board, then the TLV7022/TLV7042 in the DSG package would be possible replacements (but do something about the floating inputs). If you can change the board, consider a smaller, single-channel device like the TLV7021/TLV7041/TLV7081, or even a comparator with integrated reference voltage like the TLV4021.
Hi Frank,
remove C133 and especially C127. Low pass filtering the +input of comparator when introducing hysteresis is counterproductive. The positive feedback shall help to move through the no man's land at the trip point with increased speed. But low pass filtering ruins this effort.
And I don't like C148. The TS2431 becomes instable when the filter capacitance doesn't fit with the cathode current. See figure 15 of datasheet. Why not increasing C148 to >1µF? This would also help for the power-up issue.
Kai
hi Kai,
if I add C148 to 1uF, the waveform from simulation would look like below. the waveform looks strange when in- >in+.
BR,
frank
Hi Frank,
If VBUS is less than 5V, then you may wish to try the new LM393LV, which has a R-R input and known power-on state.
Paul,
thanks.
but unfortunately LM393LV doesn't have DSG package.
They can use TLV7042DSGR, right?
BR,
frank
Hi Frank,
Just beware that the micropower TLV7042 is almost 4x slower than the LM139 - if response time is an issue.
They may want to look at the TLV7022DSG, which is faster than the LM139, if needed.