This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I am looking at the circuit on page 50 of this presentation (Microsoft PowerPoint - Sec2_RemoteSysMonitor_Print.ppt (ti.com)). I am unable to understand the reason for use of this battery and the 2k resistor here. Would really appreciate if you could help me out.
Hello,
The TLC339 is an open drain output comparator that requires a pull-resistor to a voltage to make the input go "high".
Without the V3 voltage source, the output would never go "high". Since it is a 5V source, the output will go "high" to 5V.