Part Number: INA301
Other Parts Discussed in Thread: INA303, INA302
Hi,
Can you please share INA301A3 spice model which includes RESET functionality?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey Sadashiva,
We currently do not have the INA301 spice model with RESET functionality, the current model was designed with ALERT pin being in the transparent mode all the time. We apologize for the inconvenience and will work to update the model.
If a simulation is needed immediately, the INA302A3/INA303A3 can be used in place of INA301A3 as it is very similar in performance. The only real difference is that there is a second comparator in INA302/303 and that the RESET pin for INA301 is the LATCH pin for INA302/INA303.
Sincerely,
Peter