Part Number: PGA309EVM-USB
Other Parts Discussed in Thread: PGA309
Hi Jon,
I am getting a difference in results when I make a switch from using Vref_int set at 4.096V to using a Vref_ext supplied at 4.096V.
I am not sure why I am getting the results I am getting.
I modified your model file (7212021_e2e_modelfile_modified.txt) and precal file (7212021_e2e_precal_modified.txt) that were provided to answer our original question to use an external Vref rather than the internal Vref.
My modified model and precal files are test-121313-rtp-Vref_ext-model.txt and test-121313-rtp-Vref_ext-precal.txt. These files are attached here.
[Filenames] Pre-Cal Filename=test-121313-Rtp-Vref_ext-precal.txt Sensor Emulator Filename=7212021_e2e_sensorfile_modified.csv [Misc] Comments=test, rtp, vref_ext Serial No=8003 Model No=2001 Model ID=test-vrefext Use Sensor Emulator=TRUE
[PGA309_Settings] Numb Reg=3 Poly Order=2 Output Mode=1 Vout_High_Target=4.500000 Iout_High_Target=0.000000 Iout_Low_Target=0.000000 Vout_Low_Target=0.500000 Vs=5.000000 Vref=4.096000 Calibrate Nonlin=FALSE Reg0=0 Reg1=0 Reg2=0 Reg3=3072 Reg4=0 Reg5=0 Reg6=5151 Reg7=0 Reg8=0 Temp0=-1.111000 Temp1=23.889000 Temp2=54.444000
The sensor emulator file remained the same (7212021_e2e_sensorfile_modified.csv).
6470.7212021_e2e_sensorfile_modified.csv
I am providing a comparison of the Vref_int versus Vref_ext results in the attached Excel file '210902-Question on setup for Vref_ext.xlsx'.
The Excel file shows the the jumper settings that are used on my PGA309 test board for the Vref_ext configuration.
It also shows the parameters used in your Vref_int precal file and my Vref_ext precal file.
Screen shots of the Auto-cal, EEPROM and Block Diagram are provided for the Vref_int and Vref_ext configurations.
210902-Question on setup for Vref_ext.xlsx
Thanks for your help.
Regards,
Frank