Part Number: LM9044
Hi,
For LM9044, need to know the default output during STB/STG event:
As per the datasheet, LM9044 has gain of 4.5
And it has feature for open connection (or cold sensor) detection by providing default output of ~2V.
Can you please provide some information on below cases:
Case 1: If during STB = 28V event occurs (inputs are clamped to 14V), the output will saturate to Vcc (i.e. 5V) as gain is 4.5. Please confirm
Case 2: If STG occurs, means input will be at 0 potential, output will be approx = 4.5 * some offset = ~200mV to 300mV which happens to be the case in Lean mixture (or RICH) also.
If Case 1 understanding is correct, default o/p will be 5 and can be used as to detect the STB event.
Is there any way to detect STG events?
Regards,
Sunney