Part Number: LMH6628QML-SP
Other Parts Discussed in Thread: LMH6628, OPA837, OPA858
Hello, for a new design I need a buffer in a redundant configuration. Therefore, I want to combine the output of two LMH6628 components. Only one of the two components will be powered at a time. To avoid back currents into the output of the unpowerd component I want to use diodes. For compensation of the diode voltage drop the diodes shall be integrated in the feedback path.
Q1: Is this a suitable configuration?
Q2: Is there an application note that describes the preferred architecture for a redundant op-amp buffer architecture?
Best regards Markus