Part Number: OPA2131
Hi team,
Is clamp diode or input protection circuit integrated in OPA2131?
OPA2131 datasheet does not explain this. Is there any way to judge whether the amplifier is integrated with clamp diodes?
Best Regards,
Amy Luo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2131
Hi team,
Is clamp diode or input protection circuit integrated in OPA2131?
OPA2131 datasheet does not explain this. Is there any way to judge whether the amplifier is integrated with clamp diodes?
Best Regards,
Amy Luo
The absolute maximum ratings for the input voltage imply that there are clamping diodes from GND and to VCC. (See [FAQ] Can the input voltage (Vi) to my logic device be higher than the supply voltage (Vcc)?)
In other words, the amplifier OPA2131 ( IN to V+, IN to V- ) is internally integrated with a clamping diode, isn't it?

Hi Amy,
Yes, your highlight above shows that there are diodes to the supply voltages (V- and V+). There are no diodes, however, between the inputs (-IN, +IN). So, the input differential voltage ((+IN) - (-IN)) is not limited by diodes, as is the case for many amplifiers. For this device, the voltage on the inputs is only limited to be between the supply voltages.
Let me know if this answers your question.
Regards,
Mike