This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there, I am currently using the PGA308EVM and am trying to test several gain values but am running into a problem where the Set Vin value is not being read properly by the software and USB DAQ. For example, I have Auto Vin Vdif set to 10m and Vcm set to 2.5. When I click Read Vin it is displaying -61.59m, and does not change when Auto Vin is changed. Could the ADC on the USB DAQ be faulty?
Hi Kanisius,
I will need to get a hold of a PGA308EVM in the lab, and attempt to reproduce the issue.
I expect I will get back to you in a business day by Monday end of Day US time.
Thank you and Regards,
Luis
I have resolved the issue. I connected JMP9 and JMP 10 to ADS- and ADS+. Also connected JMP6 to ADS1.