Other Parts Discussed in Thread: INA139
Hi TI support Team,
Good day.
We have been using INA138 for quite some time, but recently the current reading detected from production is getting higher.
I would like to know the current range reading calculation will just base on gm highest = 202uA/V Typ = 200uA/V Min = 198uA/V ?
Rs = 2mOhm
RL = 200KOhm
| IS | Vout (Typ) | Vout (Min) | Vout (Max) | Good Part | Within Specification | Faulty Part | Out of specification |
| 0.3 | 0.024 | 0.02305 | 0.02472 | 0.0231 | OK | 0.038 | NG |
| 0.6 | 0.048 | 0.0461 | 0.04945 | 0.0462 | OK | 0.062 | NG |
| 0.9 | 0.072 | 0.06916 | 0.07417 | 0.0693 | OK | 0.093 | NG |
| 1.7 | 0.136 | 0.13063 | 0.14011 | 0.135 | OK | 0.152 | NG |
| 3.2 | 0.256 | 0.24589 | 0.26373 | 0.246 | OK | 0.271 | NG |
| 4.6 | 0.368 | 0.35346 | 0.37912 | 0.361 | OK | 0.39 | NG |
| 6.1 | 0.488 | 0.46872 | 0.50274 | 0.48 | OK | 0.509 | NG |
| 7.7 | 0.616 | 0.59167 | 0.63461 | 0.599 | OK | 0.628 | NG |
| 11.4 | 0.912 | 0.87597 | 0.93955 | 0.896 | OK | 0.927 | NG |
Based on the calculation, the previous batch we have used is all within the calculation, however the recent batch INA138 calculation is all out of the range. would it be normal?
| Measure by Meter (A) | Measure by Good Part (A) | Measure by Faulty Part (A) |
| 0.3 | 0.342 | 0.564 |
| 0.6 | 0.533 | 0.876 |
| 0.9 | 0.916 | 1.269 |
| 1.7 | 1.662 | 2.014 |
| 3.2 | 3.173 | 3.515 |
| 4.6 | 4.663 | 5.016 |
| 6.1 | 6.164 | 6.527 |
| 7.7 | 7.665 | 8.028 |
| 11.4 | 11.433 | 11.815 |
Seem like the new batch IC is having higher reading compare previous batch IC.
any advise on this?
Thank you
Ben