This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP7300: the part dosnt work like data sheet.

Part Number: LMP7300

im using the lmp7300 in a very simple way with no hysteresis:

 

where in my case, Rpullup=8.25kohm, and vcc=5V. 

I enter to in+ a triangular wave like the following:

and I see that vin_h and vin_l are 0.986V instead of 2.048V. the prob is very accurate and Iv checked all the things related with scaling and accuracy.  

what is the problem?