Part Number: OPA818
Other Parts Discussed in Thread: OPA855
Hello,
I had asked on this topic before, unfortunately it seems I am not able to make this measurement successfully. I have a TIA with 5kohm gain that connects to a bare die with a high speed photodiode (which is bonded to the pcb). We have the desired signal around 1-50 MHz. According to the PD manufacturer, the diode should have sub pF capacitance and since we only need maximum 50 MHz, we added a 33pF C to limit the bandwidth.

The big yellow block on the left would contain the photodiode, and closes the loop. In our test board, we don't have the photodiode yet and we close the loop on the PD Bonding PCB via a 0 ohm resistor. Since the capacitance of the diode should be small compared to the 33pF we have on the inverting input of the 818, I was hoping we could test the circuit without it. Unfortunately, I am not able to get good agreement to the transimpedance gain I expect (5k) ~ 74 dB. We have MMCX connectors so have clean transition to our VNA cables. We chose 1nF and 4pF for the "current divider caps" and matched input and output to 50 ohm.
The s-params look as follows:

Can anyone provide some guidance on how we can get back to the transimpedance curve from this?
Any help would be greatly appreciated!
best regards
Dominik