This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4531: ths4531

Part Number: THS4531

Dear TI-san,

 

I decided to use a microphone"A" with an output impedance of 5.2kΩ and set resistance of the amplifier input to 8.2kΩ.

8.2kΩ is intended to minimize power supply noise of connected laptop computer.

 

After that, I changed from microphone"A" to microphone"B", so I was allowed to discuss change of op amp peripheral circuit with E2E.

And I understand that 8.2kΩ of microphone amplifier input resistance was obtained with consent TI-san.

 

The manufacturer of microphone"B" insists on changing input resistance of microphone amplifier from 8.2kΩ to 82kΩ, which is 10 times larger.

The rationale is that output impedance of microphone"B" is 5.5kΩ.

 

Please let us know your opinion.

 

 

Thanks,

S.Suzuki