Part Number: OPA615
Other Parts Discussed in Thread: OPA860
Hi,
In peak detector with OPA615, it is used BAT17 Schottky diodes at C_Hold pins. Is there any special reason for these diodes?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you klaas69. In my circuit, i have 10ns pulses which has differenf amplitude depending rise and fall times of the AGC_In signal. And with these signals, i want to measure the peak value of my signal (AGC_Out). My frequency is 20KHz .My circuit is below.

Is there any mistake in my circuit?
Hi User,
could work:

The simulation shows the performance for several amplitudes of input signal.
And here the small signal performance:

Kai
Thank you Kai. As i see in the graphic, the pulse width is about 170ns. Is this the minimum pulse width or can i apply 10ns pulse?
The OPA615 isn't so well suited for 10ns pulses:

But the OPA860 could do:

In any case, with such fast pulses the peak value versus amplitude linearity will degrade.
Kai
Thank you for your OPA860 circuit. This is better for me. Does your design require one or two OPA860?
And the last question I don't know to take multioutput at TINA (100mV, 200mV, etc) Could you write me how to do?
Hi User,
the diamond transistor and the buffer are both in one OPA860 chip. So you need only one OPA860.
To get multi outputs, go to "Analysis", "Select Control Object", click with left mouse button on the component you want change and then choose the parameter you want to change:

Kai