Part Number: LMV324
Hi,
I have a design of an Op. Amp. in a follower configuration, made it for use in the previous stage of an ADC input. The circuit, is the following

The circuit was tested on another desing using the IC LMV324AIDR, and it work great.
On a new manufacture, the LMV324AIDR was out of stock, so I made the decision to replace it with the LMV324IDR (I check out all the datasheet, and I didn't notice any big difference) . When the boards arrive, I tested the circuit, and I notice that the output of the LMV324IDR have a saturation on a high level in 2.69 V aprox. (The Op. Amp. Supply it's 3.3V). Is these behaviour correct? I check the datasheet again and didn't find any information related to these issue.
BR,
Mauro