Part Number: LMH6702
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The data sheet repeatedly emphasizes the size of the load impedance, 100 ohms, 50 ohms, etc., can the sch I use adapt to the use of different loads?
Hi Ao,
I'm sorry, I don't fully understand your question.
But if you think you can solve the instability by the choose of a certain load resistance, then I'm afraid to say that the instability can only be cured by a redesign of the layout of LMH6702.
Hey, the LMH6702 is a 1.7GHz OPAmp 1.7GHz is 1700MHz! With such a HF OPAmp every millimeter of copper tracks count. And the green circled copper track is way way way too long.
Kai
What is the carrying capacity of this circuit? Will instability occur under different loads?
Hello Ao,
Stability can be affected by a selected load; are you asking for particular guidance on understanding how to use LMH6702, or do you have specific loads or 'carrying capacities' which you are concerned about?
When designing your circuitry, the LMH6702 circuit will depend on the size, type, and other parameters of the load you are driving. You can design a circuit which accommodates various loads, but the performance may not be as good as if you designed for a single load value.
Kai's advice on your layout is also important; your design will be affected by unnecessarily long traces and other PCB layout decisions.
Best,
Alec