Part Number: BUF802
Other Parts Discussed in Thread: BUF602
Hi. I am confused a bit by the PSPICE model for this part; I am attempting to use the model in another SPICE simulation tool and the model appears to not have any definition for 2 pins on the part, as well as some other minor 'discrepancies'.
The biggest issue: the pin listing in the datasheet (https://www.ti.com/lit/gpn/buf802) lists the pins AUX_BIAS (6) and R_Bias (7), though neither of them appear in the SPICE/.LIB file. Why is that?
Elsewhere, I note that the Datasheet lists distinct input and output stage power pins, whereas the .LIB file makes reference to what I presume are combined supply pins Vcc and Vee. Not a huge deal, and anyway I see that in the notes under Table 5-1: Pin Functions on page 3 that there is reference to "Vso and Vs should be tied to the same potential since they are internally connected to each other through back-to-back diodes." Fair enough, I can deal with that.
I also see the a TEMPC pin, and some other signs that this model is really related to a schematic. How do I get a "fully pinned" model?