Part Number: OPA549
Other Parts Discussed in Thread: TINA-TI, LM3464, TPS92518, TPS92692
hi team,
My goal is to source a constant current of 1A to 15A using two OPA549s in one high power LED continously. (The specifications of the LED are shown in the figure.)
The figure below is a circuit using two OPA549s in parallel. (I Refered to the suggestions in the datasheet..)
Since I only use constant current, I want to keep the voltage fixed and control the ILIM as a DAC.
Actually I already implemented a 0.5-6A constant current source in the same way using one OPA549 and it works just fine.
(The additional circuit is configured as shown in the figure, and this circuit has an accuracy of less than 1mA if the drift caused by temperature is ignored.)
My concern is that the datasheet provides two parallel figures of OPAMP, but it's hard to find material or reviews implementing them. From some of the stuff I've checked, they all seem to be struggling and not exactly resolved.
Before I build the actual circuit, I need as much information as possible to consider. Maybe in the part of implementing my purpose "Voltage controlled continously constant current source <Vmax=5V, Imax=15A (the best if up to 20A)>", I think that the method of using the OPA549 may not be suitable. Actually 15A is considering the specs of 2 OPA549s, 20A is better for me.
to sum it up,
1. In the above configuration, what am I missing or something to consider?
2. Any suggestions from TI that are more efficient or effective for my purposes?
Thank you.
hoo