This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a few questions for the TIDA-00879 Analog Front End section.
1-) What is the formula for calculating the voltage divider resistance values so critical in the TIDA-00879 reference design chart?
2-) A capacitor is connected in parallel to the voltage divider resistors and a fixed 470pF and 510pF are connected to some voltage divider resistors together with a parallel adjusted capacitor. How are these capacitor values calculated? I marked the capacitors with yellow color in the attached picture.
Thanks,
Arge
Hi Arge,
hhm, isn't this self explaining? These are frequency compensated voltage dividers. R19 and R13 set the pace with a division factor of 1.1. The other voltage dividers perform division factors of 11, 110 and 1100, all differening from each other by a factor of ten. Becaues of being a simple voltage divider the lower resistor of the voltage divider follows the rule:
R_lower = 10M / (factor - 1)
with R_upper = 10M.
->
1.1: R_lower = 10M / 0.1
11: R_lower = 10M / 10
110: R_lower = 10M / 109
1100: R_lower = 10M / 1099
And because the 100M is in parallel to all "R_lower" the following resistors have to be mounted in parallel to the 100M:
R_lower / (1 - R_lower / 100M )
->
1.1: -
11: 1010101R
110: 91827.36R
1100: 9100.009R
And the frequency compensation is done by setting the cap in parallel to "R_lower" to give a time constant of R19 x C27 = 10M x 100p x sec = 1msec.
Kai