Part Number: OPA991
Hi,
Good Day. I have a customer who is working with OPA991. Please see below his query for your reference. Thank you very much.
Q1. OPA991. We have an application where we'd like to use an OPA991, powered with 5VDC and GND in an unity gain configuration (G=1). The output is connected to a comparator thru a 10K resistor. Input voltage will be 0 to 20V, max. input current limited to 90 uA. Vin is much higher than the positive rail. I'd like confirmation that the output will be clamped to the 5V rail when the input voltage exceeds that rail, without phase reversal at max. 20VDC.
The assumption is that the output will follow the input for Vin 0-5V and be 5V for 5V<Vin<20V.
Q2. How soon will the output of OPA991 come out of saturation from the 5V rail when the input voltage drops to zero? The data sheet freq. response indicates 1us to 0.1% but this is a different situation with only 5VDC supply and heavy overdrive on input vs. the supply.
Best Regards,
Ray Vincent