I have a situation where I cannot determine what is causing my iso124 op amp to fail. Its input side is powered from +/-12VDC and has an isolated +/- 12VDC converter to power its output side. The Vin ranges from 0-5VDC. The Output drives a 1K resistor that is used to vary a reference output. which varies the output of a power supply. During normal operation I have recently blown 5 of these iso124 devices. There are 3 other ones in my system used for other functions that are working properly( connected to the same power rails). Any ideas?
thanks,
B. E.