Part Number: THS3092
Other Parts Discussed in Thread: CDCE925
Hello
I am using CDCE925PWR to generate 19.3Meg Hertz Square wave. to feed into this THS3092. As soon as I turn on the opamp, I am seeing everywhere in the circuit that I have 260mV peak to peak in every DC input I have. I have 5Volts input from wall adapter to go into 3.3V LDO, and 1.8V LDO. I am seeing this(figure3) everywhere in the circuit. I ran fft and the frequency component of it was multiple of 19.3Meg hertz. I am able to operate Pll and generate this squarewave without this fluctuation, but just when I connect this to the THS3092 I am seeing this type of fluctuation. In figure 4, I am getting correct input and output wave. I am really confused why this might be happening. I have been stuck at this problem for weeks, and would you please help me out?
Thank you