Part Number: OPA4192
Other Parts Discussed in Thread: OPA4387, OPA4376
Hi Expert,
Customer found output noise issue with OPA4192.
Circuit : voltage follower.
V+=5V, V-=0V
This noise seems to come from power supply noise(1MHz). It has same frequency with 5V rail switching ripple.
So it is depend on PSRR performance.
But, they didn't find this issue in case of OPA4387(same circuit)
They checked the PSRR graph in datasheet. PSRR of Both device is around 22dB at 1MHz.
Is there any spec to cause of the output noise that is same freqency with power supply ripple other than PSRR?
Also, PSRR graph have different test condition between OPA4192 and OPA4387.
OPA4192 : +/-18V
OPA4387 : +/-2.75V
Does it affect PSRR performance? Also do you have any PSRR data at V+=5V, V-=0V?
Thanks
Mukuno