Part Number: BUF802RGTEVM
Hello,
I saw in this thread that a BOM would be available soon. Can I get it?
Want to see the type of LICC capacitors used.
Thanks, Ken
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BUF802RGTEVM
Hello,
I saw in this thread that a BOM would be available soon. Can I get it?
Want to see the type of LICC capacitors used.
Thanks, Ken
Hello Ken,
Thank you for looking into this using other E2E threads. The BOM was shared offline in that instance. Below is the BOM for the BUF802RGTEVM in two different file formats:
Best Regards,
Sima
Thanks for the BOM Sima!
Sadly the LICC caps LLL185R71A104MA11L are Last Time Buy, so I will be using an alterative.
The LLL185R71A104MA11L are 100pH and have +33dB insertion loss at 1GHz.

Found these 3 terminal caps with better insertion loss (-56dB at 1GHz or about 20pH), ie. lower impedance; NFM18PS105D0J3
And they are low impedance over a wider frequency range.

Best regards, Ken