Part Number: THS3001
Other Parts Discussed in Thread: THS3491, THS3091
I need to build a current booster amplifier that has voltage gain=20dB. I.e. input signal=2.5V pk-pk, output signal=25V pk-pk. I want to use THS3001 loaded with push-pull final stage. The load impedance=5ohm. The feedback signal is applied from the push-pull output to the inverting input of THS3001. Rf=560 ohm, Rg=62 ohm. Vcc=+/-17.5V Is it possible?