Other Parts Discussed in Thread: THS4509, THS4551, THS4541, THS4509EVM
Hi,
I'm Beomyu Park, in RF developement team, Samsung electronics.
I have a question about evaluation module(THS4509).
I'm finding a evaluation kit for measurement of analog baseband circuit, and I find a evaluation module (name : THS4509 evaluation module).

To minimize a loading effect of evaluation module, i will use higher register values of RG and RF for high input impedance.
In your datasheet, a RG and RF values are 100ohm and 348ohm respectively(10dB gain),
but i want to use RG register values of 2.2Kohm and RF register value of 2.2Kohm(0dB gain) or 4.4Kohm(6dB gain).
And the evaluation module will drive a differential 150ohm register load.
In this case, i want to get a below performance.
1. up to 200MHz 3dB BW.
2. up to -60dBc 2nd and 3rd order-harmonic distortion in 160MHz.
3. up to -60dBc 2nd and 3rd order-intermodulation distortion in 160MHz.
4. under 25nV/root(Hz) Input noise voltage density in 100kHz.
In addition, a VCM of DUT is 500mV ~ 600mV, so i will use a Vs+ of 2.5V and Vs- of -2.5V.
Is there any problem using evaluation module??
If you know higher performance evaluation module, please recommoned it.
Power consumption is don't care.
Best Regard.
Thank you.
Beomyu Park.