Other Parts Discussed in Thread: TAS2505, TAS2110, TAS2562, TAS2780
Hi,
I am looking for advice on a class d audio amplifier BTL configuration.
I need it to drive a purely resistive load. The load is non-linear and can vary between 2-10 Ohms or 4-20 Ohms. 1W.
the output needs to be filtered so there is no/minimal overshoot from the PWM, and the inductors should be as small as possible, so I think a high PWM frequency is needed. I also read that some integrated noise suppression exists.
I will be driving it with a MCU to generate the signal in, so a digital input amplifier may be a nice option.
There are so many options out there I was hoping for some guidance.
Kind regards,
Matt