Part Number: OPA3S2859
Other Parts Discussed in Thread: ADS1285, , REF7025
Our application is a ratiometric one, where the signal of interest is Sample/Reference. We need to connect to photodiodes where the ratio of the two varies over a large dynamic range (six orders of magnitude). Rather than using a voltage reference IC, the Reference channel is fed directly into the ADC, thereby measuring Sample/Reference directly.
We are designing using the ADS1285. Output from the ADS1285 will be ±2.5V centered on +2.5V DC. Data rates are less than 1K SPS, and we are using a single 5V analog supply (AVDD) based on the TI TPS7A2050. Digital supply is 3.3V based on the TI TPS7A2033.
Neither cost nor power is important, but we are trying to minimize noise wherever possible.
We plan on using the OPA3S2859 as for several reasons:
· It offers low input impedance to the ADS1285
· Running both Sample and Reference through a single die will minimize noise.
· Its selectable gain should help in spanning the dynamic range.
I have a few questions:
· Have we chosen the best op-amp given our project definition?
· Is there a simple way to bias the DC output of the OPA3S2859 to 2.5 AV?
· I’m assuming that the answer to the previous question will involve a 2.5V reference. I'm currently producing a common mode voltage of 2.5V using a voltage divider from a very clean AVDD. Would using a REF5025 reduce noise? Would a REF7025 further reduce noise past that?
· Since both Sample and Reference will be using the same voltage reference in biasing the output, do I need to worry about crosstalk?
Thanks,
Patrick