Other Parts Discussed in Thread: TLC27M7
Hi,
Usually datasheets mention the max Junction temperature under ‘Absolute max rating’. The formula usually used for determining the junction temperature is Tj = Ta + (Rja * power).
For TLC27M7ID:
Tj and Rja data is unavailable in the datasheet.
Max power rating is available for different packages.
But I cant use the above formula to determine the Absolute Max junction temperature coz there are 2 unknowns ie Tj and Rja.
For SN74AC14DR:
Tj and Max power rating is unavailable in the datasheet.
Thermal impedance Rja is available for different packages.
But I cant use the above formula to determine the Absolute Max junction temperature coz there are 2 unknowns ie Tj and Power.
Please specify the Maximum Junction temperature rating for these 2 components.
Regards,
Shwetha P