This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have question to ask about LMV331
The circuit design is as follows
When V+ > V-, Vo = VCC
When V+ < V-, Vo = GND
But an abnormal phenomenon occurs, when V+ < V-, Vo = VCC
Test 14pcs, normal 7pcs, abnormal 7pcs
Is there a problem with the design?
thanks
Thanks James for your post and Clemens for your support.
As Clemens correctly noted, there is a problem with the circuit since the comparator does not have an input stage that is rail to rail. One thing also worth pointing out is that in the case of a comparator, the common mode range applies to both inputs independently. For the LMV331 to operate properly where the output reflects the input conditions, both inputs need to be a minimum of 0.8V below VCC. In your use case of VCC = 3.3V, both inputs need to be less than 2.5V.
Chuck