This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA228_237_238EVM: Firmware Update Unsuccessful

Part Number: INA228
Other Parts Discussed in Thread: INA228

I'm currently using INA228 EVM with SCB connected with it. After GUI showing the status of "device connected", pop up message showing "firmware update required". After selecting "load firmware" option, 4 LEDs (D1, D2, D3 & D4) on SCB blink for three times and OFF, error message of "Flash Unsuccessful" shown. 

Had tried this approach:
- Send the command 'bsl' on the SCB's USB Serial (COM) port. Same behavior as the LEDs blinking and USB is disconnected then.