This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
I have been working on LM324N IC for doing LC Colpitts oscillator. my inductor pot core coil value is 220uH. I have tried basically all the op amp circuits related to Colpitts Oscillator that are available on the internet. kindly help on this one
Regards
Seshadri
Hello Clemens Ladisch,
thanks for your reply at very short notice. the schematics is attached here. i tried replacing L value to 220uH and tried to change capacitors for various values. the frequency obtained based on calculation is 100khz to 300khz.
thankyou,
regards,
Seshadri.L
100 mH or 100 µH? Power supplies?
You have set an amplification of more than 21. This would require an opamp with a GBW of 5 MHz. If you really want to use the LM324, try R2/R1 ≈ 3.
Hi Clemens Ladisch,
Once again thankyou for your reply at short notice. Can you suggest any circuit for getting minimum frequency with Inductor value being 220uH using LC Oscillator. kindly help on this one.
regards,
Seshadri.L
What power supplies do you have available? Do you need a sine wave or a square wave?
DC power supply.
Need to do the tank circuit with inductor coil ( L = 220uH ).
Need sine wave.
thank you
regards
Seshadri.L
Hi,
a Colpitts oscillator -especially in this frequency range- is usually built with a transistor and not with an OPAmp like the LM324.
Kai