Part Number: LF298
Hi,
We are testing LF298M for a basic S&H Application. We are using +/- 15V for supplies to measure a signal range of 0-10V.
Logic reference is connected to GND and 5V signal is given as logic high.
Whenever logic pulse is given output is fixed at -15V .
I saw a similar thread for LF398 and posting this message. I am using the same schematic given in the first page of the schematic.
Please do support on this issue.
Thanks and Regards,
Nagendra Kumar