Part Number: LMH6521
I want to use the two independent amplifiers of LMH6521 to integrate and design a DIP switch adjustable amplifier. But after design, the signal can be output from OUTA+ and OUTA-, and then connected to INB+ and INB-, but the same circuit, the signal cannot be output from OUTB+ and OUTB-. When I disconnect the A level and directly connect the signal to INB+ and INB-, I can't get the output. Can you help me see where the design of the schematic diagram is unreasonable? Thanks.