Part Number: OPA810
why VM1 is not the same as VM2?opa810.tsc

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Liping,
There is an error in the bias supplies connected to the amplifier. Please change V- to 5V so VEE is -5V and the circuit will start working as desired. In the present configuration, the amplifier's total supply voltage is 0V and it is not powered up.
Regards,
Bharat Agrawal
Yes, you are right. One more question, do you have any suggestion if I want to move the cut off frequency to higher?

Hello Liping,
This low-pass cut-off of 1.38MHz is due to the thevenin equivalent resistance (Rth) of input divider ~50M and input common-mode capacitance of OPA810 of 2 pF. There can be two ways to push this cut-off to higher values:
1. Reduce input resistors proportionally to get the same attenuation but lower Rth and higher filter cut-off.
2. If 1Mohm DC impedance is absolutely necessary, you may try realizing an all pass response by adding capacitors in parallel with input resistors such that R1C1=R2C2. Now by default C2 is 2 pF (internal to OPA810) which gives much much smaller C1 not possible to realize on the board. Hence, we use a 1 pF in parallel with 950kohm and scale up the capacitor C2 (including the 2pF from OPA810).

Here is the input impedance and gain response vs frequency:

As can be seen the cut-off frequency increases to 121MHz but the input impedance reduces with increase in signal frequency (10kohm at 16.73 MHz).
Regards,
Bharat Agrawal